sBoot Failure Transition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sBoot Failure Transition

跳至解决方案
673 次查看
Irshad2225
Contributor III

Hi, 

Is there any configuration to perform transition to 'Boot to Safety' when sBoot returns E_NOT_OK?

Currently, Mode selector is in bootloader. and sBoot is in application. 

How can the transition be achieved? Is it via configurations? Or any sBoot APIs available?

In Safety Manual, it's mentioned as hardware transition. 

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
529 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Irshad2225 

Sorry for late reply.

1. Is there any configuration to perform transition to 'Boot to Safety' when sBoot returns E_NOT_OK?

[A]: The transition mentioned is an abstract flow, no clear configuration is implemented. 

2. How can the transition be achieved? Is it via any configurations? Or any sBoot APIs available?

[A]: You could trigger reset or change the code flow(such as change PC pointer) to complete the transition, there is no sBOOT API available.

 

BR

Chenyin

在原帖中查看解决方案

0 项奖励
回复
3 回复数
530 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Irshad2225 

Sorry for late reply.

1. Is there any configuration to perform transition to 'Boot to Safety' when sBoot returns E_NOT_OK?

[A]: The transition mentioned is an abstract flow, no clear configuration is implemented. 

2. How can the transition be achieved? Is it via any configurations? Or any sBoot APIs available?

[A]: You could trigger reset or change the code flow(such as change PC pointer) to complete the transition, there is no sBOOT API available.

 

BR

Chenyin

0 项奖励
回复
649 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Irshad2225 

Thanks for your post.

I am working on your questions, may I know if you are referring to the diagram below:

chenyin_h_0-1753348864372.png

 

BR

Chenyin

 

0 项奖励
回复
646 次查看
Irshad2225
Contributor III

Irshad2225_0-1753360950374.png

 

0 项奖励
回复