s32g3 pfe firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32g3 pfe firmware

Jump to solution
1,457 Views
jiajun_cheng
Contributor III

Dear NXP fellows:

I'm currently developing Ethernet related functions and I'm looking at "S32G3_LinuxBSP_42.0_Release_Notes.pdf", The firmware specified by pfe is version 1.8.

jiajun_cheng_1-1735026793900.png

But after I burned fsl-image-auto-s32g399ardb3.sdcard into the sd card, I saw that there was already a pfe firmware, so do I need to manually replace the pfe firmware from the official website with the one in the bsp?

root@s32g399ardb3:~# ls /lib/firmware/
s32g_pfe_class.fw  s32g_pfe_util.fw  sja1110_uc.bin

S32G-VNP-RDB3 

 

 

 

0 Kudos
Reply
1 Solution
1,451 Views
chenyin_h
NXP Employee
NXP Employee

Hi, @jiajun_cheng 
Thanks for your post.

The FW you found from the pre-built images could be the same version shown in the release notes, you may not need to manually update the PFE FW if using the default image.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
4 Replies
1,399 Views
Wzlinux
Contributor III
Hi @jiajun_cheng
您好,非常抱歉我用中文询问您。
我看您的描述是您编译了42.0后就自动有了PFE的firmware。但是我按照github里面的https://github.com/nxp-auto-linux/auto_yocto_bsp/tree/release/bsp42.0 方法编译后,发现并没有启动PFE firmware. 您知道是那里出错了吗?我尝试使用如下方式后再次使用bitbake 编译
DISTRO_FEATURES_append += "pfe"
NXP_FIRMWARE_LOCAL_DIR = "/path/to/firmware/binaries/folder"
但是这种方式报错了。
ERROR: Variable DISTRO_FEATURES_append file: /home/bin/fsl-auto-yocto-bsp/build_s32g399ardb3/conf/local.conf line: 27 contains an operation using the old override syntax. Please convert this layer/metadata before attempting to use with a newer bitbake.

请问您知道如何处理吗?谢谢
0 Kudos
Reply
1,397 Views
jiajun_cheng
Contributor III

Hi, @Wzlinux 

我没有自己编译yocto,用的是官网的提供的bsp包,但是刚刚看到 @chenyin_h 已经回复了您的消息,应该可以按照他说的步骤重新编译

0 Kudos
Reply
1,452 Views
chenyin_h
NXP Employee
NXP Employee

Hi, @jiajun_cheng 
Thanks for your post.

The FW you found from the pre-built images could be the same version shown in the release notes, you may not need to manually update the PFE FW if using the default image.

 

BR

Chenyin

0 Kudos
Reply
1,448 Views
jiajun_cheng
Contributor III

Hi, @chenyin_h :

Yes, that makes sense.Thank you very much

0 Kudos
Reply