s32g2官方板官方demo多核启动失败

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32g2官方板官方demo多核启动失败

1,298 次查看
diyid007
Contributor I

1.EB导入Integration_Reference_Examples_S32G2_2023_06bootloader工程,修改app地址和大小,参考的map文件和bin文件。

2.修改luanch.bat内的正确本地路径后,编译生成bootloader.bin文件。

3.创建IVT,导出blob.bin。

4.使用flash tool擦除flash并进行烧写,在地址为0x0处烧写blob.bin,在0x20000处烧写DIO例程的bin文件。

5.更改拨码开关进行上电操作,打印如下,但LED并未点亮。

0 项奖励
回复
5 回复数

1,137 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @diyid007

I noticed that this case is similar to the private cases generated from your side, you may continue updating the case from that private channel if needed.

Sorry for the inconvenience.

Best Regards

Chenyin

0 项奖励
回复

1,243 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @diyid007

Thank you for the question.

My initial suggestion is to check the SW11[1], if it is not modified from the default value, please set it to ON and have another try.

0 项奖励
回复

1,196 次查看
diyid007
Contributor I

I am currently starting both A-core and M-core programs simultaneously, burning blob. bin at ox00000, fip.bin at 0x10000, and M-core LED program at 0x200000. Finally, when I power on, only A-core has started, but the LED still does not start properly.

0 项奖励
回复

1,198 次查看
diyid007
Contributor I

The status of SW11 is ON, but the LED still does not light up.

0 项奖励
回复

1,297 次查看
diyid007
Contributor I
 
0 项奖励
回复