s32g2官方板官方demo多核启动失败

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32g2官方板官方demo多核启动失败

955 Views
diyid007
Contributor I

1.EB导入Integration_Reference_Examples_S32G2_2023_06bootloader工程,修改app地址和大小,参考的map文件和bin文件。

2.修改luanch.bat内的正确本地路径后,编译生成bootloader.bin文件。

3.创建IVT,导出blob.bin。

4.使用flash tool擦除flash并进行烧写,在地址为0x0处烧写blob.bin,在0x20000处烧写DIO例程的bin文件。

5.更改拨码开关进行上电操作,打印如下,但LED并未点亮。

0 Kudos
Reply
5 Replies

794 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @diyid007

I noticed that this case is similar to the private cases generated from your side, you may continue updating the case from that private channel if needed.

Sorry for the inconvenience.

Best Regards

Chenyin

0 Kudos
Reply

900 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @diyid007

Thank you for the question.

My initial suggestion is to check the SW11[1], if it is not modified from the default value, please set it to ON and have another try.

0 Kudos
Reply

853 Views
diyid007
Contributor I

I am currently starting both A-core and M-core programs simultaneously, burning blob. bin at ox00000, fip.bin at 0x10000, and M-core LED program at 0x200000. Finally, when I power on, only A-core has started, but the LED still does not start properly.

0 Kudos
Reply

855 Views
diyid007
Contributor I

The status of SW11 is ON, but the LED still does not light up.

0 Kudos
Reply

954 Views
diyid007
Contributor I
 
0 Kudos
Reply