hi, nxp, how to get the example projects based on lwip and freeRTOS ?
The RTD package has been installed, but i can not find the lwip or freeRTOS example projects.
If I want to create new project based on lwip or freeRTOS or some other SDK , which package should I install ?
If the question is about S32G2, all available demos for LWIP and FreeRTOS are
parts of the main packages, S32G FreeRTOS and S32G TCP/IP Stack.
None is available above that. Refer to the documentation of each package for details.
If you are looking for software for a different SoC, post your questions in
the appropriate Forum.
Best Regards,
Platon
As it has already been explained, the examples you are looking for are parts of
their respective main packages. Install both FreeRTOS and TCP/IP packages as
specified in each package Release Notes. Study
S32DS\software\PlatformSDK_S32XX_2021_12\stacks\tcpip\examples\S32G274A\description.txt
and
S32DS\software\PlatformSDK_S32XX_2021_12\FreeRTOS\examples\S32DS\FreeRTOS_Toggle_Led_Example_S32G274A_M7\description.txt
on how to build and run TCP/IP and FreeRTOS examples, respectively.
All paths above are relative to the S32 Design Studio installation directory.
Best Regards,
Platon
We don't know how to download the related software package of LWIP or FreeRTOS.
A lot of package of S32DS was installed, but still can not find the related demo of LWIP or FreeRTOS.
Could you please provide us some clue how to download the related demo or packages of LWIP and FreeRTOS ?
Thank you very much .
You have to install the following packages: Real Time Drivers, FreeRTOS, TCP/IP stack, in that order.
Use online Automotive Software Package Manager and download all mentioned above packages in a bundle to ensure version compatibility:
Study the documentation enclosed with the bundle and each package Release Notes for installation steps.
Best Regards,
Platon