lwip and freeRTOS related examples

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lwip and freeRTOS related examples

7,048 Views
nioer
Contributor I

hi, nxp, how to get the example projects based on lwip and freeRTOS ?

The RTD package has been installed, but i can not find the lwip or freeRTOS example projects.

If I want to create new project based on lwip or freeRTOS or some other SDK , which package should I install ?

nioer_0-1644908757970.png

 

0 Kudos
Reply
6 Replies

7,025 Views
bpe
NXP Employee
NXP Employee

If the question is about S32G2, all available demos for LWIP and FreeRTOS are
parts of the main packages, S32G FreeRTOS and S32G TCP/IP Stack.
None is available above that. Refer to the documentation of each package for details.

If you are looking for software for a different SoC, post your questions in
the appropriate Forum.

Best Regards,
Platon

 

0 Kudos
Reply

7,019 Views
nioer
Contributor I

hi, NXP, we could not find the example from the package of LWIP or FreeRTOS on S32G2.

could you give us some links or package links? 

Thanks .

0 Kudos
Reply

6,991 Views
bpe
NXP Employee
NXP Employee

As it has already been explained, the examples you are looking for are parts of
their respective main packages. Install both FreeRTOS and TCP/IP packages as
specified in each package Release Notes. Study

S32DS\software\PlatformSDK_S32XX_2021_12\stacks\tcpip\examples\S32G274A\description.txt

and

S32DS\software\PlatformSDK_S32XX_2021_12\FreeRTOS\examples\S32DS\FreeRTOS_Toggle_Led_Example_S32G274A_M7\description.txt

on how to build and run TCP/IP and FreeRTOS examples, respectively.

All paths above are relative to the S32 Design Studio installation directory.

Best Regards,
Platon

 

0 Kudos
Reply

6,980 Views
nioer
Contributor I

We don't know how to download the related software package of LWIP or FreeRTOS. 

A lot of package of S32DS was installed, but still can not find the related demo of LWIP or FreeRTOS.

nioer_0-1645431714156.png

Could you please provide us some clue how to download the related demo or packages of LWIP and FreeRTOS ?

Thank you very much .

0 Kudos
Reply

6,964 Views
bpe
NXP Employee
NXP Employee

You have to install the following packages: Real Time Drivers, FreeRTOS, TCP/IP stack, in that order.

Use online Automotive Software Package Manager and download all mentioned above packages in a bundle to ensure version compatibility:

 

bpe_0-1645525043419.png

 

bpe_1-1645525105920.pngbpe_2-1645525149193.png

 

Study the documentation enclosed with the bundle and each package Release Notes for installation steps.

 

Best Regards,
Platon

 

0 Kudos
Reply

6,986 Views
nioer
Contributor I

hi, we could not find the Install both FreeRTOS and TCP/IP packages, what is the package number?

v3.4.1? or other? Could you give us a link to download the packages?

0 Kudos
Reply