""
I set the IP address of "pfe0" interface to 192.168.1.123,
and my computer IP address is 192.168.1.200.
computer is the iperf3 server, and S32G-VNP-RDB2 board is client, like picture shows, why so many Retr ?
command on board, like this:
$ ifconfig pfe0 192.168.1.123 up
$ iperf3 -c 192.168.1.200
note: Board bandwidth is 2.5Gbps, but computer is 1000Mbps.
Physically connectS32G-VNP-RDB2 P2 A/B to my computer RJ45 port..
Hello, @liujialu_2024
Thanks for your post.
I suggest trying increasing the send/receive socket buffer sizes by using the -w option, with which the Retr could be near 0, with also the 1G throughput.
BR
Chenyin