goldvip sample project file.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

goldvip sample project file.

ソリューションへジャンプ
3,086件の閲覧回数
youngdae
Contributor III

Hello

I use S32G-VNP-RDB2.

I am testing using GoldVIP-1.1.0.

If you look inside the C:\NXP\S32G2-GoldVIP-1.1\GoldVIP-1.1.0-binaries\binaries folder,

There are boot-loader and goldvip-gateway.bin file, but the sample project cannot be found.

Can you provide sample project files and source code to me?

youngdae_0-1652871812840.png

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,051件の閲覧回数
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,078件の閲覧回数
asap
NXP Employee
NXP Employee

hi youngdae,

you may refer to the GoldVIP developer's guide,  chapter 2.1 boot and chapter 2.6.2 CAN gateway provided all the basics. for the code, you could try .../NXP/GoldVIP1.x.x/configuration/ (here below showing what I have got with GoldVIP1.1.0 installed)

asap_1-1652876823942.png

last but not least, in the S32G GoldVIP trainign academy, you found CAN gateway session. in the S32G training academy, you could find S32G2 boot training slides and also LLCE CAN support training. fyi.

 

Albert
0 件の賞賛
返信
3,064件の閲覧回数
youngdae
Contributor III

Thank you for reply.

 

but don't open Project using S32DS.

This is EB Tresos Project.

How to change S32DS Project.

0 件の賞賛
返信
3,052件の閲覧回数
nxf45013
NXP Employee
NXP Employee

Hi, @youngdae,

Currently, there is no support for S32DS in GoldVIP projects. Only Tresos is supported.

Vlad 

0 件の賞賛
返信
3,044件の閲覧回数
youngdae
Contributor III

Thanks for your kind reply.

0 件の賞賛
返信