gcc error---Pfe_demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gcc error---Pfe_demo

1,854 Views
peko
Contributor I

halo,

       我在编译Pfe demo工程时遇到此问题,问题截图如下: 

企业微信截图_17053022415056(1).png

我尝试进行了多次编译器路径修正以及软件重新安装,均无效果,请问有没有解决方案?

我的环境如下:Rtd:PlatformSDK_S32XX_4_0_0

                          Eth_Pfe:Eth_43_PFE_TS_T40D11M10I0R0

                          S32ds:3.5

beat regard

 

0 Kudos
Reply
4 Replies

1,800 Views
chenyin_h
NXP Employee
NXP Employee

Hello,  @peko

We feel glad to hear that, welcome.

 

0 Kudos
Reply

1,813 Views
chenyin_h
NXP Employee
NXP Employee

Hello, Thank you for the question.

May I know if you have strictly followed the version pointed out from the document? From the document, SW32G_RTD_4.4_3.0.2, PFE-DRV_S32G_M7_MCAL_BETA_0.9.7(Eth_43_PFE_TS_T40D11M09I5R0), EB Tresos 27.1.0, gcc-9.2-arm32-eabi(from S32DS) are needed.

It seems not clear in your post.

0 Kudos
Reply

1,803 Views
peko
Contributor I

hello,Thank you for your answers.

This question is sovled.There seems to be some problem with the makefile 

0 Kudos
Reply

1,851 Views
peko
Contributor I

哦,再补充一下,我是看这篇文档进行操作的.

0 Kudos
Reply