device in S32Gx family with MacSec (IEEE 802.1AE) support ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

device in S32Gx family with MacSec (IEEE 802.1AE) support ?

跳至解决方案
1,112 次查看
SSyb
Contributor III

Hello all,

is there a device in the S32Gx family (or alternatively another family, but for automotive use), that supports MACSec (IEEE 802.1AE) ?

Or are there plans in the NXP pipeline for such support ?

 

Thanks and best regards,

Stefan

 

P.S.: a MACSec enabled automotive ethernet switch would also do for our purpose if it is found on a S32x eval board of any kind - I had checked the SJA1110, but that does not have MacSEC AFAIKS.

0 项奖励
回复
1 解答
1,098 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what we can see under the available documentation, there is no roadmap for adding MACsec under the S32Gx family. We do apologize.

We are seeing that MACsec PHY variants are under development, but no defined roadmap on when we should be able to see it.

Automotive Ethernet Switches & PHY Transceivers Brochure (nxp.com)

We can recommend asking your local NXP representative/FAE, to see if they could have more information that the one we can look into.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,099 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what we can see under the available documentation, there is no roadmap for adding MACsec under the S32Gx family. We do apologize.

We are seeing that MACsec PHY variants are under development, but no defined roadmap on when we should be able to see it.

Automotive Ethernet Switches & PHY Transceivers Brochure (nxp.com)

We can recommend asking your local NXP representative/FAE, to see if they could have more information that the one we can look into.

Please, let us know.

0 项奖励
回复
1,082 次查看
SSyb
Contributor III
ok, Thanks ! Then we'll be waiting what PHYs will be relased with MacSec