Write-protection support of eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write-protection support of eMMC

898 Views
Shenghao
Contributor III

Dear Sir,
Could you help to provide a document about eMMC deep dive such as AN13563(QSPI deep dive)?
Customer would like to study how to do the write protection on eMMC.
Thanks

0 Kudos
8 Replies

872 Views
Shenghao
Contributor III

Hi Tushar,

I've got AN13563, it is for QSPI.

Could you help to share a Deep Dive document of eMMC?

Thanks.

 

0 Kudos

842 Views
nxf92355
NXP Employee
NXP Employee

Hi Thomas

There are no document like Deep Dive of eMMC. i am not sure, let me ask to our internal team. i will update here as soon as i got update about your quarry. and can you share which eMMC you are using ?

 

 

0 Kudos

773 Views
Shenghao
Contributor III

Hi NXP,

Do you have any comment or document for it?

Thank you.

0 Kudos

629 Views
nxf92355
NXP Employee
NXP Employee

Hi Thomas

There are no such document, but you can refer document of eMMC, like "JESD84-B51".

 

Regards ,

Tushar

0 Kudos

759 Views
nxf92355
NXP Employee
NXP Employee

Hi Thomas Liao

As i said there are no document like Deep Dive of eMMC. i am waiting for conformation from team. i will get back as soon as possible, thank you for your patience

 

Regards ,

Tushar

 

0 Kudos

831 Views
Shenghao
Contributor III

Hi Tushar, 

It is MTFC32GAZAQHD-AAT we are using.

Thomas

0 Kudos

881 Views
nxf92355
NXP Employee
NXP Employee

Hi Thomas Liao


Hope You are doing well

do you want document AN13563 (QSPI deep dive) ?


Regards ,

Tushar

0 Kudos

854 Views
Shenghao
Contributor III

Hi Tushar,

I've got AN13563, it is for QSPI.

Could you help to share a Deep Dive document of eMMC?

Thanks.

0 Kudos