Which version of PFE firmware support s32g274a BSP33?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which version of PFE firmware support s32g274a BSP33?

Jump to solution
1,446 Views
ZeusChen
Contributor II

Hi NXP Community,

I downloaded the "PFE-FW_S32G_1.5.0.zip".

According to "S32G2_LinuxBSP_32.0_User_Manual-1.pdf", I put "s32g_pfe_class.fw" & "s32g_pfe_util.fw" in some where, and modify the conf/local.conf.

But I got the debug message after boot:

[    4.300371] pfeng 46000000.pfe: Firmware .elf detected
[    4.300374] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
[    4.300379] pfeng 46000000.pfe: Uploading CLASS firmware
[    4.300385] pfeng 46000000.pfe: BMU_EMPTY_INT (BMU @ p0x(____ptrval____)). Pool ready.
[    4.300389] pfeng 46000000.pfe: Selected FW loading OPs to load 8 PEs in parallel
[    4.320858] pfeng 46000000.pfe: Unsupported firmware detected: Found revision 1.5.0 (fwAPI:92367c0e25f21f49217a9b08168ad2c8), required fwAPI e1cb376b67fa4d1de800b132b328b42c
[    4.320886] pfeng 46000000.pfe: Classifier firmware loading the PE failed: 22
[    4.320894] pfeng 46000000.pfe: Error during upload of CLASS firmware: 22
[    4.321059] pfeng 46000000.pfe: HIF3 not enabled, skipped
[    4.321067] pfeng 46000000.pfe: HIF2 not enabled, skipped
[    4.321072] pfeng 46000000.pfe: HIF1 not enabled, skipped
[    4.321079] pfeng 46000000.pfe: HIF0 not enabled, skipped
[    4.321530] pfeng: probe of 46000000.pfe failed with error 5

I think I downloaded the wrong PFE firmware.

Which version of PFE firmware should I use?

0 Kudos
Reply
1 Solution
1,429 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Under the BSP33.0 Release notes, the compatible FW versions are provided. The following image is shown in the document:

DanielAguirre_0-1686679007318.png

Which indeed shows that PFE FW 1.3.0 is the one compatible with BSP33.0.

Please, let us know.

View solution in original post

2 Replies
1,436 Views
ZeusChen
Contributor II

Hi NXP Community,

As the log:

[    4.320858] pfeng 46000000.pfe: Unsupported firmware detected: Found revision 1.5.0 (fwAPI:92367c0e25f21f49217a9b08168ad2c8), required fwAPI e1cb376b67fa4d1de800b132b328b42c

 

I check the "PFE-FW_S32G_1.5.0_ReleaseNotes.pdf":

PFE_firmware.JPG

The correct PFE firmware version for me is 1.3.0.

Am I right?

0 Kudos
Reply
1,430 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Under the BSP33.0 Release notes, the compatible FW versions are provided. The following image is shown in the document:

DanielAguirre_0-1686679007318.png

Which indeed shows that PFE FW 1.3.0 is the one compatible with BSP33.0.

Please, let us know.