Which accelerator framework faster on s32g3 hw for eth-can ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which accelerator framework faster on s32g3 hw for eth-can ?

2,939件の閲覧回数
fengxianeric
Contributor IV

Hi, I see 2 sw stack as eth2can and ipcf/llcecan,  both of them are software accelerator framework,  which one is faster if we transmit large messages from Acore to Mcore to handle with ?

Welcome discussion with me.

 

0 件の賞賛
返信
3 返答(返信)

2,914件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Hope You are Doing Well

First Make Clear IPCF and LLCE both are different things. If you want to Send Massage From A core to M Core, IPCF is used. Inter-Platform Communication Framework (IPCF) is a subsystem which enables applications, running on multiple homogenous or heterogenous processing cores, located on the same chip or different chips, running on different operating systems.

While LLCE does not make Inter-Platform Communication on cores like A to M core. Please read Application Note or Product brief of ipcf and llce.

 

Regards ,

Tushar

0 件の賞賛
返信

2,901件の閲覧回数
fengxianeric
Contributor IV
I do apologize for not describing very clearly,
I mean 2 communicating channels,
[1]A53 App--->ipcf--->M7Core LLCE can
[2]A53 App-->PFE-->M7Core Can
Which communication channel can be faster ?
THanks
0 件の賞賛
返信

2,871件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

There are no comparatively latency information. It also depend on massage. IPCF is designed for core to core communication features low-latency and tiny-footprint. It exposes a zero-copy API that can be directly used for maximum performance, minimum overhead and low CPU load.i think it 's suitable for message like communication. while pfe is packet based.

 

Regards ,

Tushar

0 件の賞賛
返信