What is the formal way to add RTD path to tresos development project so making pass ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the formal way to add RTD path to tresos development project so making pass ?

1,032 Views
fengxianeric
Contributor IV

Hello, I am integrating projects, who can tell me the right way making pass by adding RTD path to project ?  thanks.

0 Kudos
Reply
2 Replies

1,023 Views
giraffe508
Contributor IV

Hi There,

To add an RTD path to your project in Tresos, you can follow these steps:

  1. Open your Tresos project.
  2. Go to the 'Project Explorer' view, and right-click on your project name.
  3. Select 'Properties' from the context menu.
  4. In the 'Properties' window, navigate to the 'Tresos' category and click on 'Paths'.
  5. Under the 'RTD Paths' section, click on the 'Add...' button.
  6. Browse to the location of your RTD file and select it.
  7. Click 'OK' to close the 'Properties' window and save your changes.

By following these steps, you should have successfully added the RTD path to your Tresos project. If you encounter any issues or need further assistance, please refer to the Automotive Software and Tools Knowledge Base for more information and resources.

0 Kudos
Reply

1,007 Views
fengxianeric
Contributor IV

Thanks caring, I see project properties window and Resource/ConfigurationProject/ProjectPreferences/Run/DebugSettings there, and did not find  'Tresos' category (you mentioned) in EB tresos 27.1.0, Sorry for that.

0 Kudos
Reply