What is the compatible pfe firmware version of bsp35?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the compatible pfe firmware version of bsp35?

999 Views
irfank
Contributor III

We are using bsp35 and pfe1.5. It depends on release note:

irfankarazor_1-1691074481316.png

 

 

 

There is a error as seen below?

irfankarazor_0-1691074650104.png

 

 

0 Kudos
Reply
4 Replies

842 Views
irfank
Contributor III

Thanks you for your support, It was my fault.

975 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For BSP35.0, PFE-FW v1.5.0 is the one compatible with. For the log that you are showing, we see that the u-boot version is a newer one than the one we have under our BSP35.0 image:

DanielAguirre_0-1691089343184.png

For which we assume you are building your own image. How are you building your image? Can you confirm which version you are building?

Please, let us know.

0 Kudos
Reply

933 Views
irfank
Contributor III

Hello,

We compile our image by yocto. 

Start commit of our  Uboot code  is https://github.com/nxp-auto-linux/u-boot/commit/f30287c440b5371df683aac37b7521048d164d05.  then we update it depends on our board. 

If we use same uboot code under bsp33 with pfe1.3. It is ok.

But If we use this uboot code with bsp35 with pfe1.5. We have the above error.

If we use this uboot with bsp35 with pfe1.3 . uboot is bring up, but pfe is not connect network.

 

irfankarazor_0-1691131989778.png

 

0 Kudos
Reply

901 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might not be understanding. You use the BSP33.0 u-boot branch and PFE-FW 1.3 and it works, but you use your same image and BSP35.0 u-boot branch and PFE-FW 1.5 and it does not work, is this correct?

Which BSP base is your image? We understand that you are only changing the u-boot but your base image is the same, which we assume is BSP33.0, is this correct?

Please, let us know.

0 Kudos
Reply