When I use the "EB" tool to refer to "AN13750" to configure "Bootloader_S32G2XX_aSR_4.4_S7", the following error occurs and it prompts that there is no license. How can I solve it?At the same time, I have successfully imported 'SW32G-RTD-4.4_3.0.2.HF01. link' into EB
Hello, @lion_6
Thanks for your reply.
From the logs shared, seems the license is not well detected by the EB, I suggest reinstalling both EB and corresponding license administrator(removing all EB related packages first, and then reinstall 27.1 and corresponding license administrator software), furthermore, would you mind also sharing the downloading page for EB in your account? (just mask the license number)
BR
Chenyin
Hello, @lion_6
Thanks for your confirmation.
According to the AN13750,
I suggest using the EB27.1 for another trial, from my experience, most S32G software packages are developed and tested with EB27.1 version.
BR
Chenyin
Hello @chenyin_h ,
I tried downloading version 27.1.0, but still have the same problem. It seems to be a license issue and some modules are missing. Is there any other solution?
Thank you!
Hello, @lion_6
Thanks for your post.
May I know which version bootloader you are working with? also, may I know the EB version used in your work? Is it downloaded from your NXP account and had activated by the license shown in your download page?
BR
Chenyin
Hello, @chenyin_h
Thanks for the reply.
My EB version is 29.2.0
The activation status is shown in the following figure:
In terms of software, I followed the instructions mentioned in the "AN13750" manual:
SDK version: Integration-Reference_Samples_32G2_2022_06
RTD version: SW32G_STD-4.4_3.0.2HF01