Upload the CAN-GW project of GoldVIP in EB error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Upload the CAN-GW project of GoldVIP in EB error

649 Views
mmoi
Contributor II

I downloaded and installed the software package selected in goldvip1.9 through the Automotive Software Package Manager, but after loading the goldvip-gateway project, I found that these modules are   missing. Where can I get the missing modules?

微信图片_20231122104330.jpg

微信图片_20231122104333.jpg

微信图片_20231122104336.jpg

  

微信图片_20231122103847.jpg

 

Labels (1)
0 Kudos
Reply
2 Replies

614 Views
nxf92355
NXP Employee
NXP Employee

Hi mx w ,

 

Hope you are doing well

 

You can link module with EB tresos during installation time of module.

As shown below you will be ask to Choose install location for EB tresos

 

Screenshot.png

Browse the EB path like C:\EB\tresos

installation will automatically link to EB tresos

 

Or another way is copy.

For missing modules you can copy module plugins to your EB Tresos Plugins Directory (C:\EB\tresos\plugins)

For GoldVIP 1.9.0 plugins

  • Extract GoldVIP-S32G2-1.9.0-binaries.zip
  • Go to \GoldVIP for S32G2 1.9.0\configuration\s32g274ardb2\can-gw\eclipse\plugins
  • Extract plugins.zip
  • Copy and paste it into C:\EB\tresos\plugins

 RTD 4.0.1 Plugins:

  • Run SW32G_RTD_4.4_4.0.1_D2302.exe
  • Find the folder under C:\NXP\SW32G_RTD_4.4_4.0.1_D2302
  • Copy module plugins C:\NXP\SW32G_RTD_4.4_<version>\eclipse\plugins to C:\EB\tresos\plugins

 Platform Software Integration 2023_06 Plugins

  • Run Platform_Software_Integration_S32G2_2023_06.exe
  • Perform the same procedure as above

 

Best Regards  ,

Tushar

0 Kudos
Reply

624 Views
mmoi
Contributor II

Can NXP experts answer as soon as possible?

0 Kudos
Reply