Unable to setup TFTP server to connect with GOLDVIP-RDB2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to setup TFTP server to connect with GOLDVIP-RDB2

1,444 次查看
Chandan1
Contributor I

We followed S32G linux 33.4 user manual for TFTP server setup in Ubuntu 20.4.

Installed all libraries and configured Host Ip address :192.168.110.10

Installed all libraries as per the document. Target board set IPAddr(192.168.110.10) and server IP (192.168.110.20).

after ping from target device : this error came. Unable to ping.

ARP Retry count exceeded; starting again
ping failed; host 192.168.110.20 is not alive

PFE_MAC-1 Ethernet cable i connected for tftp:

Screenshot from 2023-03-21 16-40-52.png

 

How to fix the ping issue , is it issue in target or in the host configuration.

0 项奖励
回复
2 回复数

1,401 次查看
nxf92355
NXP Employee
NXP Employee

Hi Chandan

Hope you are doing well

Connected GMAC port and TFTP server via network cable.

s1.png

Please also referee Document Number: AN13185   page no 9 and 10  along with S32G-VNP-RDB2 Ethernet Enablement Guide. Hope this will help you.

 

Best Regards ,

Tushar

0 项奖励
回复

1,371 次查看
williawh
Contributor III

@Chandan1 did you get this to work? Maybe I could help if not.

0 项奖励
回复