Unable to build fsl-image-auto for Linux BSP v33

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to build fsl-image-auto for Linux BSP v33

2,042 Views
rishabh-j-dev
Contributor I

I am trying to build the fsl-image-auto for s32g274ardb2 using the Linux BSP v33. 

 

I followed the steps in the quick start guide and am running into a build error for nfs-utils. I am attaching the build error log to this ticket. Can you please take a look and see if this is a known issue? Do you know of any workarounds for it? 

This error happens as part of when I run the command bitbake fsl-image-auto

Due to this error, the image is unable to be built properly

Thanks!

0 Kudos
Reply
3 Replies

1,983 Views
nxf92355
NXP Employee
NXP Employee

Hi Rishabh

 

Hope you are doing well

Is this issue solved ?

 

thanks ,

Tushar

0 Kudos
Reply

1,963 Views
rishabh-j-dev
Contributor I

Yes, I was able to build with the patch I attached to the previous message

0 Kudos
Reply

2,019 Views
rishabh-j-dev
Contributor I

Not sure if there is a cleaner fix but I was at least able to get the compilation to go through with the following patch file. Right now, I am just disabling the warnings but there might be a better way of dealing with it. 

0 Kudos
Reply