URGENT - PFE and Bridge creation Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

URGENT - PFE and Bridge creation Support

700 Views
dramadan
Contributor II

Hello, 

 

Kindly, Bridges creation introduces high CPU load. It takes more than 1 seconds to create three bridges. We are trying to reduce this CPU load issue. We have the following questions: 

1- What is NXP expectation time for PFE bridge creation?
2- Why do we need more than one bridge to comm between A53 and M7?
3- Is the Auxuliry mandatory to communicate between A53 and M7?. If No, what are other options?
4- If more than one bridge is needed, is it possible to have Eth messages after the first one and not wait for all bridge creation?

Tags (1)
0 Kudos
Reply
2 Replies

652 Views
Aubineau_FAE
NXP Employee
NXP Employee

It is not normal to take 1 second. Can you describe in detail,  what is the relevant code you did?

0 Kudos
Reply

621 Views
Aubineau_FAE
NXP Employee
NXP Employee

Hi Doria,

Any feedback?

0 Kudos
Reply