Hi everyone,
I've built the auto_yocto_bsp release/bsp33.0 for the s32g399aevb platform.
the build is successful, however the u-boot device tree file is empty.
I checked the u-boot code in s32g399aevb-fsl-linux/u-boot-s32/2020.04-r0/git/arch/arm/dts/s32cc.dts
below is the content of s32cc.dts
/dts-v1/;
/ {
};
where can I find the u-boot device tree for s32g399aevb platform?
u-boot version: 2020.04-r0
Best Regards
Solved! Go to Solution.
Hello sami,
You should use the fsl-s32g274ardb2.dts or fsl-s32g274ardb.dtsi as base this works.
Regards
Thanks for the reply,
where can I find these files? and how to use these
I checked `s32g399aevb-fsl-linux/u-boot-s32/2020.04-r0/git/arch/arm/dts/` and I don't see these files.
Hello,
You can find the S32 BSP in:
https://www.nxp.com/app-autopackagemgr/software-package-manager:AUTO-SW-PACKAGE-MANAGER
However NXP don't hve a S32G3x BSP yet.
Regards
Hello sami,
You should use the fsl-s32g274ardb2.dts or fsl-s32g274ardb.dtsi as base this works.
Regards