The problem of setting up the development environment for S32G274A chip based on AN13750

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem of setting up the development environment for S32G274A chip based on AN13750

178 Views
lion_6
Contributor I

I want to develop the S32G274A chip and refer to the AN13750 manual for environment setup. The required GitHub link is no longer accessible. For the construction of the U-BOOT/ATF/LIUNX kernel mentioned in the manual, I referred to the "Linux BSP 42.0 User Manual for S32G2 platforms". But currently there is no software SDK for IPCF, can it be provided?
Thank you!

0 Kudos
Reply
1 Reply

165 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @lion_6 

Thanks for your post.

The IPCF package could applied from the following link:
https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER

chenyin_h_0-1750410450542.png

 

BR

Chenyin

0 Kudos
Reply