The VLAN ID is incorrect when multicast data is sent

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The VLAN ID is incorrect when multicast data is sent

2,514 Views
B0
Contributor I

The PFE driver version we used is as follows:
PFE-DRV_S32G_A53_QNX_RTM_1.0.0

In QNX 7.0 system, we configure VLAN 10 based on PFE0. The VLAN configuration method is as follows:
ifconfig vlan10 create
ifconfig vlan10 vlan 10 vlanif pfe0
ifconfig vlan10 172.16.110.11 netmask 255.255.255.0 up
However, when sending data through multicast(from 172.16.110.11  to 239.5.x.x), I capture packets through tcpdump and find that the VID is 7. How can I solve this?

Labels (1)
0 Kudos
Reply
1 Reply

2,496 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello B0,

 

This issue is from QNX i guess someone will help you, or better move to QNX forum.

 

Regards

0 Kudos
Reply