Hi Team,
We are using TJA1057GTK/3 and TJA1043TK in our design.
We would like to know if the CAN transceiver is capable of the following
1.Informing SOC when a Invalid Data (Sended) failure is detected on CAN_H and CAN_L in less than 400ms
2. To inform SOC when a Bus OFF failure is detected on CAN wire CAN_H and CAN_L in less than 400ms
3. To inform SOC when a Missing Frame failure is detected on CAN wire CAN_H and CAN_L in less than 400ms
If it is capable , how this can be verified/checked.
If not is there any provision that we could implement this feature?
Regards,
Vishal.A