Sboot FCCU Ncf Tests - Alarm Timeout Enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sboot FCCU Ncf Tests - Alarm Timeout Enable

462 Views
Irshad2225
Contributor III

Hi, 

While testing Sboot FCCU NCF tests, one of the tests is getting failed due to alarm timeout disabled. Its not available in Emecm module. 

Could you mention where exactly it can be configured?

Regards, 
Irshad

Labels (1)
Tags (5)
0 Kudos
Reply
3 Replies

437 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Irshad2225 

Thanks for your confirmation.

The CMU_SAFETY_CORES_ERROR is related to the CMU_FC checking, I have checked the FCCU settings in eMcem, it is related to the fault_28, may I know if you have correctly set it via the eMcem?

 

BR

Chenyin

0 Kudos
Reply

450 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Irshad2225 

Thanks for your post.

May I know which version SAF is used on your board? which test failed?

 

BR

Chenyin

0 Kudos
Reply

449 Views
Irshad2225
Contributor III
Hi Chenyin,

SAF version: SW32G_SAF_2.0.2_QLP01_D2410
I have enabled only CMU_SAFERY_CORES_ERROR as R3 for test configuration.


0 Kudos
Reply