Sample application to demonstrate the LLCE-PFE Can-to-Ethernet and Ethernet-to-Can bridges

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample application to demonstrate the LLCE-PFE Can-to-Ethernet and Ethernet-to-Can bridges

3,844 次查看
salimmulla2021
Contributor III

Hello, 

I have below queries with respect to the MCAL versions:

1. Is it possible to share latest stable version of the EB, LLCE, PFE and RTD?

2. is it possible to do flashing via S32 Flash tool?

标记 (1)
0 项奖励
回复
7 回复数

3,833 次查看
nxf92355
NXP Employee
NXP Employee

1. Is it possible to share latest stable version of the EB, LLCE, PFE and RTD?

-> you need software account for same.

2. is it possible to do flashing via S32 Flash tool?

-> yes , you can flash

标记 (1)
0 项奖励
回复

3,828 次查看
salimmulla2021
Contributor III

Hello,

I have NXP account and everything. So, request you to provide details of the version information and steps for flashing without debugger. 

 

0 项奖励
回复

3,813 次查看
nxf92355
NXP Employee
NXP Employee
If you have software account , then you can directly see version information for same.
got to as below image and click on Software account >  view account
 
Screenshot from 2023-05-03 12-16-37.png

 

Regards ,
Tushar
0 项奖励
回复

3,784 次查看
nxf92355
NXP Employee
NXP Employee

did got version and s32G flash tools pdf ?

0 项奖励
回复

3,778 次查看
salimmulla2021
Contributor III

I got the PDF but Could you please let me know how to convert the generated elf file to bin file and what are the placements of IVT image or is that possible to flash elf file?  As per below ticket there is no S2DS project for PFE.

Re: CAN2ETH and ETH2CAN LLCE example for S32DS - NXP Community

 

0 项奖励
回复

3,769 次查看
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

To generate .bin file , Read S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE. Read from page number 19 which describes steps to generate .bin file . IVT setup also describes. I attached that guide please refer it.

Thanks & Regards,

Tushar

0 项奖励
回复

3,822 次查看
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

Please read S32_Flash_Tool_User_Guide.pdf. it available at location  NXP/S32DS.3.4/S32DS/tools/S32FlashTool/doc/

Thanks & Regards,

Tushar

0 项奖励
回复