S32G399A-RDB3, WKUP21 configured as wakeup source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G399A-RDB3, WKUP21 configured as wakeup source

跳至解决方案
2,752 次查看
wjb
Contributor I

Can NXP provide register settings/steps to set WKUP21 as wakeup source?

board = NXP S32G399A-RDB3

Thank you

-w

0 项奖励
回复
1 解答
2,533 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The following information is provided under the BSP38.0 User Manual:

DanielAguirre_0-1707936311248.png

Don't know if it helps.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
15 回复数
2,598 次查看
Bramo
Contributor I

Have you checked out the documentation provided by NXP for the S32G399A-RDB3 board?

0 项奖励
回复
2,738 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Are you looking into setting this under the M7 core (Real-Time Drivers related) or the A53 core (Linux related)?

If for M7 core, can you help us share the RTD package version you are using?

If for A53 core, can you help us share the BSP version you are using?

As for the general request, are you looking for the general steps? Or for example codes?

On regards of the general steps, we can recommend looking into the Chapter 23 Wakeup Unit (WKPU) of the S32G32 RM [Page 967, S32G3 Reference Manual, Rev. 3, 02/2023].

Please, let us know.

0 项奖励
回复
2,737 次查看
wjb
Contributor I

A53 core

We are running a QNX BSP, but maybe you could provide the register setting steps for S32G399A-RDB3, as was provided in this previous request to NXP for s32k platform:

https://community.nxp.com/t5/S32G/Standby-and-Wakeup-by-RTD-on-S32G2/m-p/1522874

Thank you,

-Bill

0 项奖励
回复
2,731 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for the feedback. We see that the post relates to S32G, for which we assume the S32K was a typo. If so, we will share the registers related to S32G3 for WKUP21 similar that what was shared under the referenced thread:

WKPU_WIFER = 0;
WKPU_WBMSR = 0x00100000;
WKPU_IRER = 0x0;
WKPU_WRER = 0x0;
SIUL2_0.MSCR[183].B.PUE = 1;
SIUL2_0.MSCR[183].B.PUS = 1;
SIUL2_0.MSCR[183].B.IBE = 1;
STBY_GPR.WKUP_PUS.B.WKUP_PUS |= 0x00100000;
WKPU_WIPUER_WIPDER = 0x00100000;
STBY_GPR.WKUP_PUS.B.WKUP_PU_OVERRIDE |= 0x1;
WKPU_WIFEER = 0;
WKPU_WIREER = 0x00100000;
WKPU_IRER = 0;
WKPU_WRER = 0x00100000;
WKPU_WISR = 0xffffffff;

Still, could be that we misunderstood the request. If so we apologize.

Please, let us know.

0 项奖励
回复
2,724 次查看
wjb
Contributor I

On S32G399A-RDB3 board, I am utilizing J5 pin 19 as wakeup source, labeled:
GPI[182]
WKUP21
External IRQ7

Would settings of:
WKPU_WBMSR
STBY_GPR.WKUP_PUS.B.WKUP_PUS
WKPU_WIPUER_WIPDER,
WKPU_WIREER
WKPU_WRER

= 0x00200000 ?

then set MSCR[182]:
SIUL2_0.MSCR[182].B.PUE = 1;
SIUL2_0.MSCR[182].B.PUS = 1;
SIUL2_0.MSCR[182].B.IBE = 1;

Thanks, -bill.

0 项奖励
回复
2,721 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We do apologize, it does seem that we provided the wrong values. As you say, MSCRn should be 182:

DanielAguirre_0-1707409489385.png

And for the hex, it is also correct, should be 0x00200000:

DanielAguirre_1-1707409538235.png

Again, we do apologize for our mistake.

Please, let us know.

0 项奖励
回复
2,719 次查看
wjb
Contributor I

With the recommended settings, J5 pin 19, WKUP21 reads 3.3v.
1) run mode (not standby), low to WKUP21 set the following register as expected:
WISR = 00200000
2) standby mode, WKUP21 immediately drops out (no longer 3.3v)
board remains in standby

Shouldn't this pin retain its value in standby?

0 项奖励
回复
2,682 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If done correctly as shown under the S32G3 RM []:

DanielAguirre_0-1707495378794.png

The pull-up should have been changed to the WKUP module and it should still be enabled (since there is still voltage under the VPRE_3V3 power rail).

Can you debug your application? If so, can you stop prior to requesting the mode change under MC_ME_MODE_CONF? Then read the values of related the registers to confirm the values.

Please, let us know.

0 项奖励
回复
2,617 次查看
wjb
Contributor I

I verified the following:

                                         before_standby     after_standby
WKUP21                          High                       Low
VPRE_3V3                       High                      High
PMIC_STBY_MODE_B   High                       Low
VDD_IO_STBY                High                       High

Note:
It appears transitioning from standby to run mode is operating correctly.
The internal RTC confgured as Wakeup Source does resume HW from standby mode.

Were you able to configure and use WKUP21 as wakeup source on HW S32G399A-RDB3?

 

0 项奖励
回复
2,580 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your update. We seem to be able to maintain the pullup under WKUP21 under the RTD's (with M7 core).

How are you implementing the register configuration from your side?

We can also recommend opening a ticket under the NXP online services, for a private channel in case sharing information requires it.

Please, let us know.

0 项奖励
回复
2,577 次查看
wjb
Contributor I

I am using Trace32 (A53 core) to setup registers.

Does GPIO/Wakeup setup need to be configured by ATF, or can this be done using a Cortex-A53 EL1 driver ?

 

0 项奖励
回复
2,547 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Are you using any specific BSP version from NXP?

Under the BSP38.0 User Manual the following is told:

DanielAguirre_0-1707918747331.png

In which the modification needs to be made under the TF-A. Also, the following is noted:

"Note, however, that U-Boot is not involved in the Suspend/Resume sequence; only the TF-A is."

Don't know if this is of use.

Please, let us know.

0 项奖励
回复
2,537 次查看
wjb
Contributor I

Where can I download the TF-A source?

Thanks, -bill

0 项奖励
回复
2,534 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The following information is provided under the BSP38.0 User Manual:

DanielAguirre_0-1707936311248.png

Don't know if it helps.

Please, let us know.

0 项奖励
回复
2,515 次查看
wjb
Contributor I

Thanks for your help, appreciate it.

-bill

0 项奖励
回复