Hi,
We have a board designed with S32G399a and PVR5510AMDALES. We already have BSP31 running on this board.
We have I2C going to the PMIC (5510). We can dump the registers on 5510. But I am not clear on how to measure continuously monitor the voltage, current and power.
Appreciate any help in this regard.
thanks and best regards
Madhu
PS: I tried the 'sensors' command. But it only measures temperatures from the S32G Thermal Management Unit.
Hi @ Madhu Krishnamurthy
Thanks for using portal
As per datasheet of PVR5510AMDALES There are no provision seems to measure current , power , voltage through Registers of VR5510. you can measure externally.
There are voltage supervisor which monitors overvoltage and undervoltage occurrences . When an overvoltage occurs on a VR5510 regulator monitored by one of these pins, the associated VR5510 regulator is switched off until the fault is removed. Voltage monitoring is active as soon as FS_ENABLE=1. UV/OV flags are reported accordingly.
NOTE: this is monitoring but not measuring. please refer datasheet for voltage supervisor.
Regards
Tushar