S32G3: debugging Linux with s32 debug probe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G3: debugging Linux with s32 debug probe

1,187 次查看
s153022
Contributor III

Dear NXP Support Team,

We have recently purchased the S32G-VNP-RDB3 Board and have successfully compiled the NXP Auto Yocto Linux BSP v38.0. We can run Linux and boot to the Linux prompt without issues. Additionally, we have purchased the S32 Debug Probe.

Our current objective is to debug the Linux kernel, ATF (Arm Trusted Firmware), and U-Boot using the debugger. We seek guidance on how to connect the debugger to these components, set breakpoints within the kernel, ATF, and U-Boot code, and navigate through the debugging process.

Could you kindly direct us to a comprehensive guide or provide instructions that cover the connection of the debugger, setting of breakpoints, and stepping through the debugger?

Thank you for your assistance.

Best regards,

0 项奖励
回复
1 回复

1,169 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @contributor3

Thanks for the question.

For using the debugger, the corresponding official documents could be downloaded from the following link: (including the user guide, quick start guide and fact sheet), which could be the basics for using the debugger.

https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-debug-probe:S32-...

 

Besides, there are also some other useful posts from the community, which could help for the details.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-JTAG-Flash-Programming-with-S32-...

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Start-S32-Debugger-from-S32-Desi...

Hope it helps.

 

Best Regards

Chenyin

 

0 项奖励
回复