S32G274 use ipcf in autosar ,M7 communication with linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G274 use ipcf in autosar ,M7 communication with linux

2,670 次查看
jianqun
Contributor II

M7 运行autosar,A核使用linux

我们想使用IPCF,我已经安装了SW32G_IPCF_4.6.0_D2205

我看IPCF在EB工具上是没有配置的,是否只有在S32DS内配置后再以复杂驱动集成在autosar中呢?

如何配置和如何集成到autosar内有没有更详细的说明呢,我看了下ipcf的安装包内的doc文档,感觉看的不是很明白

The M7 runs autosar and the A core uses linux

We want to use IPCF, I have already installed SW32G_IPCF_4.6.0_D2205

I see that IPCF is not configured on EB tool, is it only configured in S32DS and then integrated into autosar with complex drivers?

Is there a more detailed description of how to configure and integrate into autosar? I looked at the doc document in the ipcf installation package and felt that it was not very clear

标记 (2)
0 项奖励
回复
7 回复数

2,637 次查看
nxf92355
NXP Employee
NXP Employee

Hi ianqun li

 

Hope you are doing well

Please  install the IPCF 4.8.0, there is a example provide to show how to configure IPCF in EB tool. you will find it at the location  SW32G_IPCF_4.8.0_D2212/eclipse/plugins/Ipcf_TS_T40D11M40I0R0/examples/EBT/S32G2/Ipcf_Example_S32G274A_M7

 

Regards ,

Tushar

 

 

 

0 项奖励
回复

2,625 次查看
jianqun
Contributor II

Hello, IPCF relies on a different version of RTD and BSP than BSP33

0 项奖励
回复

2,620 次查看
nxf92355
NXP Employee
NXP Employee

Hi

Yes, Software dependencies are RTD -> SW32G_RTD_4.4_4.0.0_D2207 and BSP-> BSP35.0

please read ReleaseNotes (SW32G_IPCF_4.8.0_D2212_ReleaseNotes.pdf) for more information

 

Regards ,

Tushar

0 项奖励
回复

2,618 次查看
jianqun
Contributor II
But we use the BSP33 version, and I see that version 4.7 also supports EB, but the RTD that he relies on is not available on your official website
0 项奖励
回复

2,617 次查看
jianqun
Contributor II

But we use the BSP33 version, and I see that version 4.7 also supports EB, but the RTD that he relies on is not available on your official website

0 项奖励
回复

2,609 次查看
nxf92355
NXP Employee
NXP Employee

Hi

Version 4.7 relies on RTD 3.0.4 .   It is available on flexera site

Screenshot from 2023-08-07 14-54-44.png

 

Regards ,

Tushar

0 项奖励
回复

2,589 次查看
jianqun
Contributor II

I can't see IPCF4.7 version in my account. At present, our S32G274 is a new project, which BSP version do you officially recommend to use, BSP35 or BSP33

0 项奖励
回复