M7 运行autosar,A核使用linux
我们想使用IPCF,我已经安装了SW32G_IPCF_4.6.0_D2205
我看IPCF在EB工具上是没有配置的,是否只有在S32DS内配置后再以复杂驱动集成在autosar中呢?
如何配置和如何集成到autosar内有没有更详细的说明呢,我看了下ipcf的安装包内的doc文档,感觉看的不是很明白
The M7 runs autosar and the A core uses linux
We want to use IPCF, I have already installed SW32G_IPCF_4.6.0_D2205
I see that IPCF is not configured on EB tool, is it only configured in S32DS and then integrated into autosar with complex drivers?
Is there a more detailed description of how to configure and integrate into autosar? I looked at the doc document in the ipcf installation package and felt that it was not very clear
Hi ianqun li
Hope you are doing well
Please  install the IPCF 4.8.0, there is a example provide to show how to configure IPCF in EB tool. you will find it at the location  SW32G_IPCF_4.8.0_D2212/eclipse/plugins/Ipcf_TS_T40D11M40I0R0/examples/EBT/S32G2/Ipcf_Example_S32G274A_M7
Regards ,
Tushar
Hello, IPCF relies on a different version of RTD and BSP than BSP33
Hi
Yes, Software dependencies are RTD -> SW32G_RTD_4.4_4.0.0_D2207 and BSP-> BSP35.0
please read ReleaseNotes (SW32G_IPCF_4.8.0_D2212_ReleaseNotes.pdf) for more information
Regards ,
Tushar
But we use the BSP33 version, and I see that version 4.7 also supports EB, but the RTD that he relies on is not available on your official website
Hi
Version 4.7 relies on RTD 3.0.4 . It is available on flexera site
Regards ,
Tushar
I can't see IPCF4.7 version in my account. At present, our S32G274 is a new project, which BSP version do you officially recommend to use, BSP35 or BSP33