S32G2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G2

259 次查看
c980-022
Contributor I

In one of our applications, when using the NXP S32G2 processor (Part Number: S32G254AABK1VUCT), is it possible to utilize two FlexRay channels, with each channel having both A and B lanes?

0 项奖励
回复
3 回复数

128 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @c980-022 

Thanks for the reply.

I suggest refering the IOMUX file attached in the S32G2_RM for details of the pin, which may like:

chenyin_h_0-1756284488935.png

 

BR

Chenyin

 

0 项奖励
回复

203 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @c980-022 

Thanks for your post.

From the S32G2 block chart:

chenyin_h_0-1756202090449.png

As marked, there are two FlexRay existed

 

BR

Chenyin

0 项奖励
回复

137 次查看
c980-022
Contributor I
Thank you for your reply. Could you please tell me that when I searched for FlexRay in the manual, I only found the pins for one of the FlexRay interfaces. Where can I find the pins for the other one?
0 项奖励
回复