S32G2 : Can't find PFE TRESOS Component on M7 core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 : Can't find PFE TRESOS Component on M7 core

6,669 Views
skseofh
Contributor II

Hi,

I'm using S32G274A

 

I installed The S32 Real Time Drivers AUTOSAR 4.4 Version 2.0.0.

But I can't find PFE TRESOS componet.

Is there any other things to do to use PFE component on M7 core?

0 Kudos
Reply
12 Replies

6,645 Views
skseofh
Contributor II

Installed : 

S32 RTD AUTOSAR 4.4 Version 2.0.0 Hot Fix 02

skseofh_0-1641426005396.png

But there is no Eth_43_PFE component in my component list:

skseofh_1-1641426096267.png

 

please let me know how to use Eth_43_PFE componet on M7 core

0 Kudos
Reply

6,630 Views
bpe
NXP Employee
NXP Employee

PFE driver for M7 core is a separate package. Use Automotive Software Package Manager  to download it:

 

bpe_0-1641472568692.png

 

Follow the documentation enclosed within the package on how to use it with S32DS

Best Regards,
Platon

 

0 Kudos
Reply

6,619 Views
skseofh
Contributor II

I've already downloaded the package PFE.

I think there is no document to follow...

 

Instead, there is release note : 'PFE-DRV_S32G_M7_MCAL_BETA_0.9.5_ReleaseNotes.txt'

And it says,

========================================================
Installation:
========================================================
This package shall be integrated with following version of NXP AUTOSAR MCAL:
  - SW32G2_RTD_4.4_2.0.0_HF02
This package uses PFE firmware:
  - s32g_pfe_class firmware version HF 1.0.1 (included in package)

There are 2 installation options after extracting files from this package:
    - Copy the directory Eth_43_PFE_TS_T40D11M09I5R0 to the plugins 
    directory of your EB tresos installation
    - Create an EB tresos link to the directory where this package is extracted

 

It is ambiguous what the 'plugins directory of your EB tresos installation' is.

And I tries to find some plugins directory and copy the directory 'Eth_43_PFE_TS_T40D11M09I5R0' to that plugins directory, but it didn't work.

 

Please let me know

1) if it is the right way to refer to this document

    if not what document should I refer?

2) If it is, where can I find the 'plugins directory of your EB tresos installation'?

    Could you give me a hint?

 

0 Kudos
Reply

6,607 Views
bpe
NXP Employee
NXP Employee

I think there is no document to follow...

The driver is packed with about 400 pages of documentation in three PDF files under eclipse\plugins\Eth_43_PFE_TS_T40D11M09I5R0\doc\:

bpe_0-1641553801755.png

 

 

1) if it is the right way to refer to this document
if not what document should I refer?

 

Plugins installation instructions can be found in Section 3.3 of the driver Integration Manual (AUTOSAR_MCAL_ETH_43_PFE_IM.pdf). The Release Notes generally describe the same steps. The both are valid.

2) If it is, where can I find the 'plugins directory of your EB tresos installation'?

 

If you don't see the plugins\ directory, install EB Tresos first. The plugins\ should be right below the folder where you installed it. If you are working with S32DS and not EB Tresos as the screen captures you posted earlier in this thread suggest, follow the steps in the Release Notes below "  Delivered as an extension for S32 Design Studio" bullet.

 

Best Regards,
Platon

 

 

 

0 Kudos
Reply

6,103 Views
MateoSegura413
Contributor III

Hey,

Could we please get an answer for this?

We want to use the PFE from the M7 cores. Is this even possible? The installation file that is downloaded, is indeed not of the same "update_site" format than everything else (RTD,RTOS, etc.). It cannot be installed the conventional way, and section 3.3 of the manual does NOT explain how to install for S32DS.

The help would me much appreciated

Thank you

@bpe 

0 Kudos
Reply

6,559 Views
skseofh
Contributor II

And I downloaded EB tresos studio.

But there is no target that I can use;;

skseofh_0-1641883468433.png

Could you let me know how to create 'Target' (S32G274A)?

0 Kudos
Reply

6,519 Views
bpe
NXP Employee
NXP Employee


The installation steps you described in your recent posts are not valid. They
fail because you they are not in line with any document discussed earlier in this
thread. The only suggestion that can be given in this regard is, review the
documentation you have been suggested, namely Release Notes for NXP
Semiconductors PFE MCAL Driver swv: 0.9.5
and S32G PFE MCAL 4.4 Driver Integration Manual Section 3.3 and do follow them
strictly.

Best Regards,
Platon

 

 

0 Kudos
Reply

6,560 Views
skseofh
Contributor II

Here is what I've done.

 - install new software

skseofh_0-1641882198904.png

- add 'PFE MCAL 0.9.6.zip' 

skseofh_1-1641882277835.png

 

But it said, "Could not find jar:file:/~~~~~~~~~~'

skseofh_2-1641882311154.png

So I open PFE zip file

skseofh_3-1641882371643.png

And this is 'LLCE SDK' that can install SDK.

skseofh_4-1641882437115.png

PFE zip contains different files that can install(like LLCE SDK)

0 Kudos
Reply

6,576 Views
skseofh
Contributor II
 If you are working with S32DS and not EB Tresos as the screen captures you posted earlier in this thread suggest, follow the steps in the Release Notes below "  Delivered as an extension for S32 Design Studio" bullet.

 

Where can I find "Delivered as an extension for S32 Design Studio"?

Could you give me more detailed info?

0 Kudos
Reply

3,568 Views
Youngsoo_do
Contributor III

we are curious about this work, too. so if you have any progress, please share.

0 Kudos
Reply

4,785 Views
Haribadri1989
Contributor II

Hi,

 

Did you find a solution? Is there a PFE software extension that can be used in S32 design studio?

0 Kudos
Reply

5,270 Views
PeaceZhang
Contributor II

Do you have any progress? 

0 Kudos
Reply