S32G multi-core application failed to run

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G multi-core application failed to run

188 Views
lion_6
Contributor I

When I set up the development environment based on AN13750, I followed the steps shown in the following figure:

lion_6_0-1751597277975.png

The following issues have occurred:
root@s32g274ardb2:~# echo 1 > /sys/kernel/ipc-shm-sample-instance1/ping
root@s32g274ardb2:~# dmesg | grep ipc-shm-sample_multi-instance
[ 63.397060] ipc-shm-sample_multi-instance: starting demo on instance 0...
[ 63.397085] ipc-shm-sample_multi-instance: INST0 ch 0 >> 19 bytes: SENDING MESSAGES: 1
[ 63.397098] ipc-shm-sample_multi-instance: send_data_msg(): failed to get buffer on instance 0 for channel ID 1 and size 32
[ 422.873017] ipc-shm-sample_multi-instance: starting demo on instance 1...

lion_6_1-1751597453613.png

 



My software versions:
BSP:33.0-5.10.109
ipcf:4.6.0_D2205

May I ask how I can solve this
Thank you!

 

0 Kudos
Reply
1 Reply

172 Views
Joey_z
NXP Employee
NXP Employee

hi,lion_6

Thank you for your information.

I checked you post a similar ticket. To facilitate providing you with support. I will support to you in this ticket. (S32G2 Run the application on S32G-VNP-RDB2 ERROR - NXP Community)

BR

Joey

0 Kudos
Reply