S32G goldbox M7 enable LLCECAN0 and LLCECAN1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G goldbox M7 enable LLCECAN0 and LLCECAN1

498 Views
vsong
Contributor II

NXP employee,

 

Can anyone help me to configure the S32G goldbox, allow the external CAN bus loop.  signal form LLCE CAN0 loop back to CAN1 (external with Canoe monitor the Bus traffic).

I have no idea how to config the I2C to enable the transceiver.  Please provide some detail steps.

 

thanks,

Labels (1)
0 Kudos
Reply
1 Reply

472 Views
nxf92355
NXP Employee
NXP Employee

Hi vivian song

 

Hope you are doing well

There is an Example named Can_Llce_Ds_Loopback_S32G274A_M7 in S32DS. please install LLCE in S32DS and after install you will see that example

There are also example for i2c in S32DS,

Hope this will help you, or tell us if you have query

 

B,R

Tushar

 

 

0 Kudos
Reply