/**
** Copyright 2021 NXP.
** This software is owned or controlled by NXP and may only be used strictly in accordance with the applicable license terms.
** By expressly accepting such terms or by downloading, installing, activating and/or otherwise using the software
** you are agreeing that you have read, and that you agree to comply with and are bound by, such license terms.
** If you do not agree to be bound by the applicable license terms, then you may not retain, install, activate or otherwise use the software.
*/
#include "stdint.h"
/* IVT binary */
const uint8_t ivt_binary[256] = {
/* HEADER */
0xd1, 0x1, 0x0, 0x60,
/* reserved_1 */
0xff, 0xff, 0xff, 0xff,
/* Self-Test DCD */
0xff, 0xff, 0xff, 0xff,
/* Self-Test DCD (backup) */
0xff, 0xff, 0xff, 0xff,
/* DCD */
0xff, 0xff, 0xff, 0xff,
/* DCD (backup) */
0xff, 0xff, 0xff, 0xff,
/* HSE */
0xff, 0xff, 0xff, 0xff,
/* HSE (backup) */
0xff, 0xff, 0xff, 0xff,
/* Application bootloader */
0x0, 0x4, 0x0, 0x0,
/* Application bootloader (backup) */
0xff, 0xff, 0xff, 0xff,
/* boot_config */
0x0, 0x0, 0x0, 0x0,
/* life_cycle_config */
0x0, 0x0, 0x0, 0x0,
/* reserved_2 */
0xff, 0xff, 0xff, 0xff,
/* hse_fw_config */
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
/* reserved_3 */
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
/* gmac */
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff,
};
MEMORY
{
int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00000000
int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x00010000
int_sram_shareable : ORIGIN = 0x22C00000, LENGTH = 0x00004000
int_sram : ORIGIN = 0x34004000, LENGTH = 0x00400000
int_sram_stack_c0 : ORIGIN = 0x34404000, LENGTH = 0x00002000
int_sram_stack_c1 : ORIGIN = 0x34406000, LENGTH = 0x00002000
int_sram_stack_c2 : ORIGIN = 0x34408000, LENGTH = 0x00002000
int_sram_stack_c3 : ORIGIN = 0x3440A000, LENGTH = 0x00002000
int_sram_no_cacheable : ORIGIN = 0x34500000, LENGTH = 0x00100000
ram_rsvd2 : ORIGIN = 0x34600000, LENGTH = 0x00DFFFFF
LLCE_CAN_SHAREDMEMORY : ORIGIN = 0x43800000 LENGTH = 0x3C800
LLCE_LIN_SHAREDMEMORY : ORIGIN = 0x4383C800 LENGTH = 0xa0
LLCE_BOOT_END : ORIGIN = 0x4383C8A0 LENGTH = 0x50
LLCE_MEAS_SHAREDMEMORY : ORIGIN = 0x4384FFDF LENGTH = 0x20
}
@nxp Thank you for your support.