Hi,All
I want to set up a new c file and gcc to make an executable file, I want to put it into the S32g274ardb2 board and test it.
But I can not find it when I boot the board use tool Tera Term, becasuse I put it into the usr/lib, but I do not find it .
I do not want to make the c file like to add kernel module, so I do not add a new layer and rebuild the linux kernel , it just like application for c, I use c library header like: stdio.h , I do not use linux kernel header:because open or close fucntion can not be found in kernel header.
I search the web and it tells me that SCP command can do it, but I do not want to use Ethernet.
Can someone tell me the steps to put the executable file into board? Or it has some way to build it into the image?
I update the c file and executable file,please help me.