Hi,
I want to test the CAN usecase.
I connected the following pins using wires:
i) FlexCAN0(L) to LLCE-CAN0 (L)
ii) FlexCAN0(H) to LLCE-CAN0 (H)
iii) FlexCAN1(L) to LLCE-CAN1(L)
iv) FlexCAN1(H) to LLCE-CAN1(H)
I executed the following script:
./canperf.sh -t can0 -r can1 -i 0 -o 4 -s 64 -g 0 -l 10
But the output was not as expected. Attaching the generated report below.
Could you please explain what could be the issue here? Is there any additional hardware requirement? The image used is golvip1.3.0
Hello, Vishnu,
The fact that the reported M7 core loads are 0% tells me that the application doesn't run at all. Are you sure you booted from QSPI? The SW4.7 DIP switch should be set to OFF.
Best regards,
George