S32G Design Studio build project from the example is not displaying

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Design Studio build project from the example is not displaying

Jump to solution
404 Views
Jayanth-KB
Contributor III

Dear NXP team,

I am facing an issue in S32DS build project from the example is not displaying [There is no reference examples] after installing all software bundles for S32G399ARDB3 

  1. HSE_Standard_Firmware_0_2_51_0
  2. Inter_Platform_Communication_Framework_4_10_0
  3. LLCE_Standard_Driver_and_Firmware_1_0_9
  4. Real_Time_Drivers_5_0_0

Hardware Setup:

Board: S32G399ARDB3

OS: Windows

JayanthKB_0-1744174632916.pngJayanthKB_1-1744174714521.png

I have reinstalled all the software bundles several but still not able see reference example for s32g vnp rdb3 board

Any help and guidance will be appreciated

Best Regards,
Jayanth KB

0 Kudos
Reply
1 Solution
378 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jayanth-KB 

Thanks for the post.

Seems you were testing it with S32DS3.6.1? which is quite new, I tested it on my end based on a S32DS3.6.0 setup, and installed the RTD5.0.0 manually from the images downloaded, the examples could be created for S32G3 successfully as follows:

chenyin_h_0-1744193599164.pngchenyin_h_1-1744193639910.png

I have checked your log, but seems the packages installed are not fully shown from your snapshot, would you mind sharing a full picture of it, to ensure if the RTD is well installed.

 

BR
Chenyin

View solution in original post

0 Kudos
Reply
1 Reply
379 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jayanth-KB 

Thanks for the post.

Seems you were testing it with S32DS3.6.1? which is quite new, I tested it on my end based on a S32DS3.6.0 setup, and installed the RTD5.0.0 manually from the images downloaded, the examples could be created for S32G3 successfully as follows:

chenyin_h_0-1744193599164.pngchenyin_h_1-1744193639910.png

I have checked your log, but seems the packages installed are not fully shown from your snapshot, would you mind sharing a full picture of it, to ensure if the RTD is well installed.

 

BR
Chenyin

0 Kudos
Reply