S32G Cortex M7 Programming / Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G Cortex M7 Programming / Flash

跳至解决方案
1,094 次查看
arun_belamge
Contributor III

Hello All.

I have been able to successfully build and generate the IVT blob for the RGB / UART example projects in the S32G DS 3.6. 

Since I currently do not have any Debugger, the only way for me to run the program is via flashing the binary using the Flash Tool.

I have tried many programs and flashed it successfully, but nothing seems to work.

Can anyone tell me where am I going wrong?

For reference,

Main Program:

arun_belamge_2-1760086058368.png

 

Linker:

arun_belamge_1-1760086017588.png

 

IVT Config:

arun_belamge_0-1760085965483.png

Flashing done on QSPI Flash memory as well as SD Card, both load the program successfully but I don't see the LEDs light up or UART print (Linflexd_Uart Example).

Thank you!

0 项奖励
回复
1 解答
913 次查看
Joey_z
NXP Employee
NXP Employee

hi,Contributor II

1.You can try to the baremetal/MCAL RTD demo using this way. 

2. You need to download the package(Integration_Reference_Examples_S32G3_2023_02) to find the file of QSPI configuration. The file foder is the (

C:\nxp\Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\res\flash), you can find it in this folder.

Also, I cannot share the project with you, due to the policy of company, sorry for the inconvenience.

BR

Joey

 

在原帖中查看解决方案

0 项奖励
回复
20 回复数
1,075 次查看
Joey_z
NXP Employee
NXP Employee

hi,

Thank you contacting us.

What is your value of intc_vector? Make sure it is right to be set.

1. You can try to refer to this link for your issue. (https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/S32G/7641/1/S32G-VNP-RDB2-SW-UG.pdf)

2.Also, make sure your project configuration correct, and please try to reduce the size of binary.

Hope this can help you.

BR

Joey

0 项奖励
回复
1,067 次查看
arun_belamge
Contributor III

Hi.

Thank you for the response.

I think i have the intc_vector value correct, please have a look.

arun_belamge_0-1760095705851.png

And I am not sure why the size is a lot more than the one given in the Enablement guide. Can you tell me what could be the reason?

Thank you!

 

0 项奖励
回复
1,057 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

Please modify the linker file , you can try to reduce the size of binary.

BR

Joey

0 项奖励
回复
957 次查看
arun_belamge
Contributor III

Hello Joey.

I made minor size changes in linker file and got the size of the binary reduced to less than 3mb, yet the program doesn't work. 

Please help!!!

arun_belamge_1-1760410814305.png

 

arun_belamge_0-1760410781339.png

Thank you.

BR

Arun

0 项奖励
回复
949 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

Do you cannot use the demo of uart on  both SD and Qspi mode?

What is your RTD/IDE version?

BR

Joey

0 项奖励
回复
945 次查看
arun_belamge
Contributor III
Hi.
Yes I have tried in both SD and QSPI flash, and neither work.
IDE : S32DS 3.6.0
RTD : S32_RTD_5_0_0_QLP03_D2505_ASR_REL_4_4_REV_0000_20250530
Thank you.
BR
Arun
0 项奖励
回复
922 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

I have helped you to test the demo of Uart_Example_S32G399A_M7 in RTD 5.0.0, and apply it to use the QSPI mode on RDB3 board. It is the process as the below.

1.Built the demo of Uart and create the .bin file in S32DS IDE. I do not modify any more, just Update Code and Built it.

2. Create the Blob.bin file. You can refer to the configuration as the following picture. 

Joey_z_0-1760426249959.png

3.Flash the blob.bin to Nor Flash and setting the hardware boot from QSPI, then open serial console to choose 9600 baterate, you can find the output information.

Joey_z_1-1760426553231.png

Hope this can help you.

BR

Joey

 

 

0 项奖励
回复
918 次查看
arun_belamge
Contributor III
Hi Joey.
Thanks for the support.
I have two questions:
1. Is this example using MCAL or Baremetal? I want to try baremetal.
2. Where can I find the QSPI configuration file?

Also is it possible for you to archive your project as is and attach here, so that i can try to run it without changing anything for testing.

Thank you!

BR
Arun
0 项奖励
回复
914 次查看
Joey_z
NXP Employee
NXP Employee

hi,Contributor II

1.You can try to the baremetal/MCAL RTD demo using this way. 

2. You need to download the package(Integration_Reference_Examples_S32G3_2023_02) to find the file of QSPI configuration. The file foder is the (

C:\nxp\Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\res\flash), you can find it in this folder.

Also, I cannot share the project with you, due to the policy of company, sorry for the inconvenience.

BR

Joey

 

0 项奖励
回复
908 次查看
arun_belamge
Contributor III
Hi Joey.
Tried this and yet after successful flash, I see no output on the UART console.
Is there anyway to know if bootloader is working but application throwing error, or vice-versa.
Should I expect any logs when bootloader fires up?
I am not sure how to debug this...

Thank you for the continued support.

BR
Arun
0 项奖励
回复
887 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Could you share your IVT configuration?

This is my S32 Flash Tool configuration, you can try to compare it, make sure your blob.bin flash successfully.

Joey_z_0-1760436141100.png

BR

Joey

0 项奖励
回复
880 次查看
arun_belamge
Contributor III

Hi Joey.

Here is the IVT config screenshot:

arun_belamge_2-1760436597540.png

 

Flashing screenshot:

arun_belamge_0-1760436544059.png

Thanks!

 

 

0 项奖励
回复
873 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Do you use the customer board or RDB3?

BR

Joey

0 项奖励
回复
870 次查看
arun_belamge
Contributor III
Hi Joey.
It's the S32G-VNP-RDB3.

BR
Arun
0 项奖励
回复
820 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Could you try to the demo of Uart_Example_S32G399A_M7 in RTD? And refer to my configuration.

BR

Joey

0 项奖励
回复
787 次查看
arun_belamge
Contributor III
Hi Joey.
I tried the Uart_Example_S32G399A_M7 with the same configurations as yours, still nothing on the console after flashing.

FYI, I am able to boot Linux BSP through SD card on the A53 core.

BR
Arun
0 项奖励
回复
775 次查看
arun_belamge
Contributor III

UPDATE

I reinstalled the S32DS 3.6 and the drivers and now I am able to run the UART Example projects.

But the LED project still doesn't work, this is my code:

arun_belamge_0-1760521119221.png

Please have a look.

Thank you.

BR

Arun

 

0 项奖励
回复
771 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

It is good news.

Do you have set the SW11 ON?

Do you have the Multimeter to test the pin?

BR

Joey

0 项奖励
回复
620 次查看
arun_belamge
Contributor III
Hi Joey.
Firstly, thank you for the continued support, highly appreciated.
LED i was simply trying to check if M7 boots and works, but since the UART example is working, I have no need for the LED example (anyways, i ll try your suggestion and see the continuity using a multimeter).
For my application I have few doubts, I think for that I will create a new thread.

Thank you.

BR
Arun
0 项奖励
回复
616 次查看
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Glad to support you.

You can post new ticket if you have any question.

BR

Joey

0 项奖励
回复