S32G BSP Build error with using yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G BSP Build error with using yocto

3,163 Views
ChenXiang
Contributor I

Hello everyone,

        When using bitbake fsl-image-auto, buiding yocto bsp error,pionting out :

        The postinstall intercept hook "update_font_cache" /"update_gtk_icon_cache"  failed

        detail info is this:

        (1) update_gtk_icon_cache ERROR

NOTE: Running intercept scripts:
NOTE: > Executing update_gtk_icon_cache intercept ...
NOTE: Exit code 127. Output:
/home/cks/s32g/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/s32g274aevb-fsl-linux/fsl-image-base/1.0-r0/intercept_scripts-18c2e18def091e750d3f1e16960804e8d4b4dc4ec55ce1a3bd63e990e798e5f9/update_gtk_icon_cache: 10: /home/cks/s32g/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/s32g274aevb-fsl-linux/fsl-image-base/1.0-r0/intercept_scripts-18c2e18def091e750d3f1e16960804e8d4b4dc4ec55ce1a3bd63e990e798e5f9/update_gtk_icon_cache: /home/cks/s32g/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/s32g274aevb-fsl-linux/fsl-image-base/1.0-r0/recipe-sysroot-native//gdk-pixbuf-2.0/gdk-pixbuf-query-loaders: not found

ERROR: The postinstall intercept hook 'update_gtk_icon_cache' failed, details in /home/cks/s32g/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/s32g274aevb-fsl-linux/fsl-image-base/1.0-r0/temp/log.do_rootfs
DEBUG: Python function do_rootfs finished

 

        (2)update_font_cache ERROR

ERROR: The postinstall intercept hook 'update_font_cache' failed, details in /home/cks/s32g/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/s32g274aevb-fsl-linux/fsl-image-auto/1.0-r0/temp/log.do_rootfs
DEBUG: Python function do_rootfs finished.

         

Thanks

Tags (2)
0 Kudos
Reply
1 Reply

3,142 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You should erase everything about yocto and restart again, this issue is very common when happens this.

 

Regards

0 Kudos
Reply