Hi NXP Community,
I am working with a fresh install of S32 Design studio v3.6.1 and created a project for S32G399A. I have also intsalled the RTD package using the "Install new Software option". When I try to access the IVT tools, the design studio crashes abruptly and it happens every time I do that. I have tried installing a previous release from March 31, 2025 which also has the same problem.
I am attaching the error log generated by the studio here.
My OS info:
Linux precision-3591 6.8.0-59-generic #61~22.04.1-Ubuntu SMP PREEMPT_DYNAMIC Tue Apr 15 17:03:15 UTC 2 x86_64 x86_64 x86_64 GNU/Linux
Java version:
openjdk 21.0.7 2025-04-15
OpenJDK Runtime Environment (build 21.0.7+6-Ubuntu-0ubuntu122.04)
OpenJDK 64-Bit Server VM (build 21.0.7+6-Ubuntu-0ubuntu122.04, mixed mode, sharing)
Could you please help me out with a fix for this issue? Let me know if you need any other information from my end.
Thanks.
Hello, @pcentauri92
Thanks for you reply.
I have checked the log you provided, it may caused by the incompatible version of JAVA, from the release notes, Java17 is recommended.
However, with further checking on the issue, I suggest not using S32DS under Linux, it is because currently, there are issues existed on supporting RTD on Ubuntu host. As a result, make the installation issue fixed would not help on further use of RTD. I suggest installing the S32DS3.6.1 on a Windows Host.
Sorry for your inconvenience.
BR
Chenyin
Hello, @pcentauri92
Thanks for the post.
From the release notes of S32DS3.6.1, the following OS are supported for S32DS3.6.1, I suggest trying installing it on the OS supported for another trial.
BR
Chenyin
Hi @chenyin_h ,
I have updated my OS to the latest version which is compatible with S32 Design studio v3.6.1 and the issue still exists as you can see below.
hi @pcentauri92 . Where you able to solve this issue?
Question: Are you using Wayland or X11 in your Ubuntu setup?
Hi @daniel_ll ,
My distribution comes with X11 by default and I have been able to use the design studio by setting the GDK_BACKEND environment variable.
export GDK_BACKEND=x11
However, fthe issu still exists without the use of that variable. My distribution version is as shown below
PRETTY_NAME="Ubuntu 24.04.2 LTS"
NAME="Ubuntu"
VERSION_ID="24.04"
VERSION="24.04.2 LTS (Noble Numbat)"
VERSION_CODENAME=noble
ID=ubuntu
Has a fix been released for this in the newer version of ubuntu (25.10) ?