S32 Debug Probe issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Debug Probe issue

1,959 次查看
nioer
Contributor I

hi, NXP, when I use the S32 Debug Probe to debug S32G274, there is some problems.

check the picture bellow.

connection is ok.

nioer_0-1648547849793.png

nioer_1-1648547893387.png

nioer_2-1648547914166.png

Could you give us some advice on how to use the S32 Debug Probe?

 

0 项奖励
回复
2 回复数

1,781 次查看
PraveenKumar_K
Contributor II

@nioer did this works for u ? 

I am also facing same kind of problem while using the S32 Debug Probe to debug S32R45 EVK.

could anyone suggest me to solve this S32 Probe issue. @nxp

0 项奖励
回复

1,877 次查看
Yi_Liu_Nxa22412
NXP Employee
NXP Employee

When you connect the S32 debug probe, please make sure:

1. PMIC set to debug mode, PMIC VR5510 won't issue reset to S32G. If the PMIC watchdog reset S32G during S32DS connecting to S32DS, it will report failure.

2. S32G at serial boot mode, the M7_0 core stay at serial boot mode.

0 项奖励
回复