S32 Debug Probe Error 102

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Debug Probe Error 102

152件の閲覧回数
Flo_
Contributor I

Hello,

I have an S32G3 device and an S32 Debug probe.
When I try to debug my project on my board (after building), there is an error.

 

Flo__0-1750938364375.png

I use S32DS 3.5 version 14

Perhaps, when I try to make the "Test connection", it succeeds.

Can you help me with what the possible issues are here? Can it be caused due to my project?

 

Best Regards

 

0 件の賞賛
返信
1 返信

133件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Flo_ 

Thanks for your post.

Error 102 is defined as a connection error, may I know if a RDB3/EVB3 or custom board is used? what are the SW settings during your test?

 

BR

Chenyin

0 件の賞賛
返信