S32-DP can't connect S32G2 M7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32-DP can't connect S32G2 M7

1,215 Views
ethan-li
Contributor III

Hi,

    Customer used S32 DS for S32 V3.4 , and installed update 1 for S32 DS V3.4, RTD V2.0.0 for S32 G2 M7 Core.

     Import RTD example Project int to S32 DS V3.4.1 and compiled , connect S32 Debug probe through USB to the EVK board, lauch the debugger, the debugger indicates that the S32G2 M7 Core can't be connected.

     What are the possible reasons for this issue?

    

ethanli_0-1729505371036.png

 

0 Kudos
Reply
3 Replies

1,189 Views
Joey_z
NXP Employee
NXP Employee

hi,ethan-li

Please make sure that the S32 Debug probe is connected to the PC normally. The information in the following picture will appear in the configuration interface USB device.

XuZhang_0-1729650633016.png

Then, connect the S32 Debug probe to the development board J48, the development board is powered normally, and click Test connection to check whether the connection is established.

XuZhang_1-1729650658505.png

Hope it can help you.

BR

Joey

 

 

0 Kudos
Reply

1,174 Views
ethan-li
Contributor III

Hi Joey,

     Thank you for your reply.

      The customer was right in the first step, and the S32-DP emulator device can be find.

      Test connection, a message indicating that "board is not connected". And customer used another S32-DP emulator, the connection is successful. 

ethanli_0-1729668311134.png

ethanli_1-1729668334423.png

ethanli_2-1729668388685.png

Tags (1)
0 Kudos
Reply

1,154 Views
Joey_z
NXP Employee
NXP Employee

hi,ethan-li

There should be a problem with S32-DP. You can try to use the normal S32-DP data cable to test it to rule out whether it is a problem with the data cable.

BR

Joey

0 Kudos
Reply