Dear NXP fellows,
I am investigating how to setup the network interfaces of our S32G399A-RDB3 based custom board. This board uses BSP 41.0.
Actually, there are 3 PFE interfaces available:
- PFE_MAC0: Connected through SGMII to the SJA1110A switch port 4;
- PFE_MAC1: Connected through RGMII-ID to a 1000BASE-T1 PHY;
- PFE_MAC2: Connected through RGMII-ID to a 1000BASE-T1 PHY.
All of these interfaces are up and running. I can assign IP addresses in different subnets for each of them and I am able to ping my laptop connected through an adapter and vice-versa.
When I took a look at one internal requirement for the configuration of the IP addresses and VLAN IDs, I saw this specification:
Server Server IP VLAN ID Port
S32G_Mcore 192.168.10.10 10 50102
S32G_Mcore 192.168.12.10 12 50102
S32G_Mcore 192.168.13.10 13 50102
S32G_Mcore 192.168.14.10 14 50102
S32G_Acore 192.168.10.11 10 50101
S32G_Acore 192.168.11.11 11 50101
S32G_Acore 192.168.12.11 12 50101
S32G_Acore 192.168.13.11 13 50101
S32G_Acore 192.168.14.11 14 50101
In this case there are a total of five subnets:
192.168.10.X, 192.168.11.X, 192.168.12.X, 192.168.13.X, and 192.168.14.X
And there are different IP addresses for the S32G M7-core and the A53 core.
All of the subnet masks are 255.255.255.0.
How can I assign a different IP address for M-core and A-core? Does it imply using PFE Master-Slave configuration?
Can our board fulfill this specification?
Thank you very much for the support.
Best regards,
Guilherme