Questions about using IPCF of S32G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about using IPCF of S32G

Jump to solution
1,489 Views
learnx
Contributor III

learnx_0-1694676819475.png

What are the differences and usage scenarios between the two types of usage described in the picture above? Can you introduce them to me, or is there a document description?

 

0 Kudos
Reply
1 Solution
1,463 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

As for difference, it seems to be related to whether the application is available within the kernel itself or available under the user-space. As for examples of both scenarios should be provided under the IPCF User Manual [v4.8.0] under Chapter 6.2 "IPCF Shared Memory Sample Application for Linux" (Linux Kernel) and Chapter 6.3 "IPCF Shared Memory User-space Sample Application for Linux" (Linux User-space).

Please, let us know.

View solution in original post

0 Kudos
Reply
2 Replies
1,464 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

As for difference, it seems to be related to whether the application is available within the kernel itself or available under the user-space. As for examples of both scenarios should be provided under the IPCF User Manual [v4.8.0] under Chapter 6.2 "IPCF Shared Memory Sample Application for Linux" (Linux Kernel) and Chapter 6.3 "IPCF Shared Memory User-space Sample Application for Linux" (Linux User-space).

Please, let us know.

0 Kudos
Reply
1,429 Views
learnx
Contributor III
thanks
0 Kudos
Reply