Question about S32G3 LLCE can2can and can2eth function kernel support version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about S32G3 LLCE can2can and can2eth function kernel support version

跳至解决方案
305 次查看
GG0712
Contributor III

Hi NXP team,

 

LLCE CAN controller start to support can2can, can2eth, ...  function from BSP38 kernel 5.15

I have lots of questions about this feature.

  1. Does S32G3 Linux kernel 5.10 support these feature?
  2. Does can2eth and eth2can support to custom ethernet switch or GMAC eth0 ?
    I can not found how to use in LinuxBSP User Manual
  3. Can I use this function without enabling m core?

 

Thanks

0 项奖励
回复
1 解答
285 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

1. No, I checked the code and it is not enabled in BSP38-5.10 kernel.

2. No, only PFE is supported.

3. Yes, it is supported, you may reference the LLCE chapter of BSP UM for details.

 

BR

Chenyin

在原帖中查看解决方案

0 项奖励
回复
1 回复
286 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @GG0712 

Thanks for your post.

1. No, I checked the code and it is not enabled in BSP38-5.10 kernel.

2. No, only PFE is supported.

3. Yes, it is supported, you may reference the LLCE chapter of BSP UM for details.

 

BR

Chenyin

0 项奖励
回复