Queries on Waking up VR5510 in normal mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Queries on Waking up VR5510 in normal mode

122 Views
Zoe_19
Contributor I

Hello,

We are using VR5510 with part no. MVR5510AMDA4ES with S32G in our project. Please help with below queries

  1. Will the PMIC starts in debug mode or normal mode by default?
  2. Can we make the PMIC wake-up in normal mode with the operating mode configuration?
  3. Do I need to set to normal mode by calling set_mode() function explicitly?
  4. In the normal mode, if the watchdog is not serviced, it will reset the S32G. So, how do we disable the watchdog at initialization? Can I do it by calling the function Pmic_DisableWatchdog() at init?
0 Kudos
0 Replies