QSPI write failure on EVB with SDK BSP43

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QSPI write failure on EVB with SDK BSP43

387 次查看
hittzt
Senior Contributor I

Hi,

 

Recently, I tested qspi boot on EVB Gen2 board, but it failed after about 10 times test.

In every test, I will write the qspi flash with the related image and then reboot the board to see the status of the board.

After abour 10 times test, the qspi flash failed with message like:

=> mtd write FIP $loadaddr                                                  
Writing 1900544 byte(s) at offset 0x00000000
Failure while writing at offset 0x0
Write on FIP failed with error -110

 Would you please help to check the issue?

 

Thanks,

Zhantao

0 项奖励
回复
1 回复

363 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks for your post.

May I know if you are using EVB(https://www.nxp.com/design/design-center/development-boards-and-designs/S32G-VNP-EVB) or EVB3(https://www.nxp.com/design/design-center/development-boards-and-designs/S32G-VNP-EVB3)?

Would you mind sharing more information about the board?(Revision, S32G2 or G3 is equipped?)

 

BR

Chenyin

 

0 项奖励
回复